Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Information regarding I/O Scanner reads when STB islands are in TEST mode.

Issue

This resolution has information for STB users that applies when an STBNIP2212 NIM interfaced island is operating in TEST mode.

Product Line
Advantys, STB

Resolution

When IO scanner functionality is being used in the PLC to enable reading of island module inputs and diagnostic data, it is recommended to have the input and output areas on separate lines within the IO scanner. Otherwise, if the island is in TEST mode, the scanner will indicate an error and inputs will not be read. This is due to the nature of I/O Scanner operation when writes are prohibited by the island. It also applies to reading the HMI to PLC area.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings