Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I change the watchdog timeout value in Unity Pro?

Issue:

How do I change the watchdog timeout value in Unity Pro?

Product Line:

Watchdog timeout, Unity Pro

Resolution:

To change the watchdog timeout value, go to the Project Brower and right click on the MAST, FAST or AUX directory and choose <Properties>. The following box appears:
Properties of MAST


The Watch Dog timeout value must be greater than the period value (specified time in which the master task must be executed).
System Bit %S11 indicates watchdog overflow. This bit is set to 1 when the task execution time becomes greater than the maximum execution time (watchdog timout value).

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)