Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PL7DIF V4.2 : Error messages when reading sections differences

Goals and Symptoms

When some differences between program sections exist, the following error message can occur: "PL7 command error: can not open a program module".

Facts and Changes

The error occurs twice, once per section. However, the content of sections will be displayed only when the errors popup is validated. This issue allows to work, it just creates a little trouble.

Causes and Fixes

The cause is known, it is due to the use of characters with accent in section names. Removing accents is resolving the problem.


Legacy KB System (APS) Data: RESL179234 V1.0, Originally authored by on , Last Edited by on
Related ranges: PL7
PL7 command error: can not open a program module