Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Mirror test for the XIP driver returns an incorrect response.

Issue
The mirror test for the 'XIP' driver returns an incorrect response.

Product Line
All versions of the XIP driver

Environment
Windows XP

Resolution
If you connect to the Premium PLC to perform an 'XWAY' mirror test with the 'XIP' driver using
the default address that appears in the 'Schneider Drivers Management Properties' window, the
result will appear to be fine.
dsfcf


When you click on the 'Start' button to start the mirror test, the following error will get returned.
dgdd


The error is getting returned because either the network ID for the remote address is is not the same
as that for the local host or the 'XIP' profile is not bound to the Ethernet network adapter card
dd


The profile for the 'XIP' driver profile gets bound to the Network Interface card by clicking on the 'Bind'
button in the 'Schneider Automation CNFXP' window.
dg


The following example, uses a remote address of '2.21.0' to connect to the PLC and the
local host 'XWAY' address of the PC is set at '2.25'.