Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
STBART0200 Copper RTD Type Specified

Issue
The purpose of this Resolution is to specify the copper RTD type used on the STBART0200 module.


Product Line
Advantys STB
STBART0200

Environment


Resolution
The STBART0200 supports copper RTD types, 10 ohms at 0 degrees C.
It does not support copper RTD types, 10 ohms at 25 degrees C.