Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where do I find the USB cable driver for the XBTZG935 cable or for HMISTU/HMISCU?

Issue
Where do I find the USB cable driver for the XBTZG935 cable or for HMISTU/HMISCU?

Product Line
Vijeo Designer
XBTZG935 USB transfer cable

Resolution
This driver is included when you install Vijeo Designer HMI editing software.
It can be also be downloaded here in this FAQ.

The file is attached as "XBTZG935Setup.zip"
Unzip the file and extract "XBTZG935Setup.exe".

Schneider Electric Nigeria

Attachment(s)
XBTZG935Setup.zip [280.32 KB]