Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the pinout of the Modicon M340 Modbus port?

The pinout of the integrated Modbus port on M340 CPU's BMXP34 1000/2010/2020 is as follows:

1
RXD
2
TXD
3
RTS
4
D1
5
D0
6
CTS
7
Vcc
8
Com
9
Shield

Legacy KB System (APS) Data: RESL187214 V1.0, Originally authored by DaSo on 07/23/2007, Last Edited by DaSo on 07/23/2007
Related ranges: Modicon M340