Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which Magelis XBT-GT HMIs supports an analog camera?

Issue
Which Magelis XBT-GTs supports an analog camera?

Product Line
XBTGT Series HMI (no longer commercialized)

Resolution
There are 4 XBTGT targets that support video:
XBTGT4340
XBTGT5340
XBTGT6340
XBTGT7340.

They all have one analog video input. Therefore, for any of these targets, you can connect one video source.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings