Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does PLC Label-it for Concept software do?

PLC Label-it for Concept will take a Concept (version 2.0 and higher) converter ASC project file and automatically create I/O labels. These labels will either show what State ram register or coil ( 0X, 1X, 3X, or 4X ) or what Symbol name is assigned to which input or output on a PLC I/O module. After the software creates the label, the user would print these on their own printer and then insert this label into the sleeve or front of the I/O module. Any module that is available in Concept can have a label printed. All labels can also be customized and resized to whatever size the user wants. The default size of the labels are designed for Quantum series I/O.


Legacy KB System (APS) Data: RESL1900 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept