Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Error "proworxaddrused.frm" when trying to open a Project after installing 'Proworx 32'

Issue
The error "proworxaddrused.frm" gets returned when trying to open a project

Product Line
All versions of Proworx 32

Environment
Windows 7, Windows 10

Resolution
This error will get returned if you updated to a patch immediately after installing 'ProWORX 32' without
rebooting the PC.

To resolve the problem,

  • Insert the installation CD and start the install process.
  • Select the repair option to perform a repair.
  • Reboot the PC.
  • Apply the patch update.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings