Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
STBXTS6610 Connector Pinouts

Issue

The purpose of this resolution is to document pinouts for the STBXTS6610 HE10 connector used with the STBDDO3705 16 Channel Outpiut module.

Product Line
Advantys, STB

Resolution


pinout1 Pinout

Causes and Fixes

See Facts and Changes for pinout information.


Legacy KB System (APS) Data: RESL190495 V1.0, Originally authored by WeDa on 12/29/2007, Last Edited by WeDa on 12/29/2007
Related ranges: Advantys STB