Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Advantys STBNIC2212 Release Notes

Issue
This Resolution contains the Release Notes for the STBNIC2212 Ethernet/IP module.


Product Line
Advantys STB
STBNIC2212


Environment


Resolution
The attached document explains:

  • Known issues with the STBNIC22112 using Exec version 2.10
  • Known documentation issues in Advantys STB Ethernet/IP Network Interface Applications Guide, part number 31008204 (English).

Attachments
Advantys STBNIC2212 Release Notes v.1.1 (July 2008)

Schneider Electric Nigeria

Attachment(s)
STB_NIC_2212_Release_notes_V1.1.zip [11.38 KB]