Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum Modbus port speed on the M340 CPU?

Modbus port speed up to 38400 baud on all CPU's with embedded Modbus ports. (ex. BMXP341000, BMXP342000, BMXP342010, BMXP342020)