Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the TSXETC100 Premium Ethernet IP module scan a Allen Bradley Control Logix PLC?

The TSXETC100 cannot scan a Allen Bradley Control Logix PLC.
The reason for this is because of a proprietary way of peer to peer communication between Allen Bradley controllers.
They use Produce and Consume tag in order to synchronize information between PLCs and do not have an assembly object that the TSXETC100 can scan.
Note: The TSXETC100 can be an adapter to a Allen Bradley controller so the Control Logix PLC can scan the TSXETC100.