Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Information about RM79696044 and RM79696014 length probes

Goals and Symptoms

Information about RM79696044 and RM79696014 length probes

Facts and Changes

RM79696044
RM79696014

Causes and Fixes

RM79696044 probe have 3 electrodes: one for common, one for minimum level and one for maximum level. 3 electrodes have the same length 100 mm. The electrodes can be cut to the desired length :
a short electrode for the maximum level, a medium for the minimum level, and a long Electrode for common. The wire length between the probe and the RM35L must be lower than 1m.
The length of RM79696014 is 1m. There is not problem to cut the probe in order to have probes with different length.