Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a RoHs version of the NOE77101 be downgraded to version 3.xx

Issue
Can a RoHs version of the NOE77101 be downgraded to version 3.xx

Product Line
140NOE77101

Environment
Windows 7

Resolution
The RoHs versions of the NOE77101 cannot be downgraded to exec firmware 3.xx because of the

differences in the internal components. Only non-RoHS NOE77101 can be upgraded from 3.xx to
4.xx and downgraded back to version 3.xx.

If you try to downgrade a RoHs version of the NOE77101, it will make the unit inoperable. When this
happens, the unit must be sent back to the factory for repair.