Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
NOE771xx shows up as an ETY410 when viewed in OS Loader

Issue
NOE771xx shows up as an ETY410 when viewed in OS Loader.

Product Line
140NOE7711x

Environment
Windows 7

Resolution

The 140NOE771xx (i.e., 140 NOE77111, etc.) shows up as an ETY410 when viewed in OS Loader.
dfbvgf


The reason the 'OS Loader' shows the NOE as an EY410 is because the NOE received a bad or
incomplete download of the exec firmware. This caused the module to be missing a hardware
identification file that tells 'OS Loader' what type of module it is connected to. When this hapens,
it defaults to the ETY410 identification.

Attempts to download a new exec will fail because the OS Loader will not allow a download
when there is a mismatch in the hardware identification

To resolve the problem, the module will need to be sent back to the factory for repair.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings