Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
TSXETY4103 Exec Version 5.4 Release Notes

Issue
This Resolution contains the Release Notes for the TSXETY4103 firmware versions 5.4, 5.2, 5.1, 5.0, 4.9, and 4.8.


Product Line
Premium
TSXETY4103


Resolution
Refer to the attached document for the complete details.

  • UPDATE 1/4/13:
    Release of version 5.4
  • UPDATE 6/28/12:
    Release of version 5.2
  • UPDATE 12/15/11:
    Release of version 5.1
  • UPDATE 5/18/11:
    Release of version 5.0
  • UPDATE 12/22/10:
    Release of version 4.9
  • UPDATE 6/16/10:
    Release Notes section version 4.8
    A correction was made to Customer Action in the title: A random ETY reboot results in the Error Log recording an error 921,
Attachments
ETY4103 Exec v5.4 Release Notes.pdf


Schneider Electric Nigeria

Attachment(s)
PremiumETYPort_v5.4_Release_Notes.pdf [76.4 KB]