Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
STBNIP2212 Advantys Ethernet NIM Gateway Configuration

Goals and Symptoms

When configuring an Advantys STBNIP2212, a gateway address with the last octet of x.x.x.255 cannot be used.

Causes and Fixes

Users must avoid using x.x.x.255 as a gateway address with the STBNIP2212.
If x.x.x.255 is required to be used as the gateway address, then the STBNIP2311 should be considered.


Legacy KB System (APS) Data: RESL203940 V1.0, Originally authored by RiCr on 11/19/2010, Last Edited by RiCr on 11/19/2010
Related ranges: Modicon STB