Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to create a Cyrillic keyboard in the Vijeo Designer?

Goals and Symptoms

The String keypad allows to enter ASCII characters; it doesn't allow to enter Cyrillic characters.
The goal of this document is to describe the different steps in order to create the Cyrillic keyboard in Vijeo Designer.

Facts and Changes

Vijeo Designer V5.1 SP2

Causes and Fixes

Assume that the regional settings are configured on the PC in order to get the Russian Keyboard.
Perform the following steps (open the attached file)

Attachments

(Removed File URL: 204276_07AA/Cyrillic_Keyboard.doc)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/6b93ea510a7fdf72c125781d00587fd5/fl_block_5/0.70E?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL204276 V1.0, Originally authored by MaLy on 01/19/2011, Last Edited by MaLy on 01/19/2011
Related ranges: Magelis XBT GC, Magelis Smart BOX, Compact PC Box & Flex PC BOX, Magelis XBT GK, Magelis XBT GTW, Magelis XBT GT, Magelis Smart, Magelis Modular iPC, Magelis Compact iPC, Vijeo Designer

Schneider Electric Nigeria

Attachment(s)
Cyrillic_Keyboard.doc [294 KB]