Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What would cause the message "the module requires a voltage capacity that isn't available from the power supply" error on a Unity Pro build when using a BMXCPS2010 power supply?

The BMXCPS2010 power supply does not have a 24 Vdc output to power any of the 24 Vdc output APS_SENSORS. This is just a warning and can be ignored because you have to use an external supply to power the modules.