Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does "basic OS loader invalid checksum" displayed on a Quantum 140CPU6XXXX indicate?

This error can be seen if there was an interruption to the Executive Flash process. Sometimes the PLC is recoverable and sometimes it is not. To recover, some of the actions listed below can be attempted. Remove any PC cards installed in the PLC and any cards other than the PLC and PS from the back plane. If available, try a different power supply and back plane.

  • Power cycle.
  • Power off, press and hold the ESC key through power up.
  • Press the Restart button next to the battery.
  • Use the OS Loader to connect to the PLC using either Modbus or MB+, set to address 1 and attempt to flash firmware.
  • Power off, remove battery, remove from back plane, let sit 120 minutes and power on.

If after the above actions the PLC does not recover, it must be returned for repair/ exchange.



Legacy KB System (APS) Data: RESL212574 V1.0, Originally authored by DaSo on 09/24/2013, Last Edited by DaSo on 09/24/2013
Related ranges: Modicon Quantum

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings