Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the recommended number of wires and AWG size for connection to a BMXFTB2820 or BMXFTB2800 ?

Issue
Need to purchase wire and need to know acceptable sizes.

Product Line
Modicon X80 IO

Resolution
The recommendation is one wire between 16 to 24 AWG.