Issue
Can the CM4XXX series detect flicker severity
Product Line
CM4000
CM4250
CM4000T
Environment
Power Quality Detection
Cause
Not all CM4000 meters can detect flicker severity
Resolution
The CM4000 and CM4250, by default, do not have the capability to detect flicker severity.
To detect flickers on these meters the Current/Voltage Module Transient (CVMT) must be installed
The CM4000T by default can detect flicker severity
Can the CM4XXX series detect flicker severity
Product Line
CM4000
CM4250
CM4000T
Environment
Power Quality Detection
Cause
Not all CM4000 meters can detect flicker severity
Resolution
The CM4000 and CM4250, by default, do not have the capability to detect flicker severity.
To detect flickers on these meters the Current/Voltage Module Transient (CVMT) must be installed
The CM4000T by default can detect flicker severity
Released for:Schneider Electric Nigeria