Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the CM2000's sampling and update rate?

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

Product Line
CM2000

Environment
Sampling Rate

Resolution
The CM2000 samples at a rate of 64 times per cycle. It looks at 4 cycles out of 60 then updates approximately once per second.