Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Create a Web Page for the ECC21 using HTML.

Issue:
User would like to understand how to create custom webpages on a ECC using HTML

Product Line:
ECC21

Environment:
Ethernet Communications Card

Resolution:
The PowerLogic Ethernet Communication Card (ECC) allows power users to view real time,
tabular information from attached devices in the form of HTML pages via a standard Web
Browser (such as Internet Explorer and Netscape.) This document teaches you the basics steps
needed to develop ECC custom pages

Schneider Electric Nigeria

Attachment(s)
How_to_Create_a_Web_Page_for_the_ECC_using_HTML- .pdf [471 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: