Goals and Symptoms
| Summary: |
| It was found that setting [OID]Reset=1 in the Citect ini file, did not reset the OIDs when the variable tags are located in an include project. I've used Open Office to modify my variable.dbf. This behaviour also exists when using the ProjectDBFAddIn macro with the 'Save Only" option. Using the "Save and Reindex" option however allowed the OIDs to be reset I'm able to reset without any problems if the variable tags are located in the main project after I've modified the variable.dbf using - Open Office - ProjectDBFAddIn macro with the 'Save Only" option |
Facts and Changes
|
Causes and Fixes
| Solution: |
| - Have the variable tags in the main project if you are using - Open Office - Use the ProjectDBFAddIn macro with the "Save and Reindex" option |
Ctiect is aware of this problem and we are currently investigating this issue.
Released for: Schneider Electric Nigeria


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.