Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the nominal current for ION6200 and ION7300?

Issue:
A user require the information on ION6200's and ION7300's nominal current.

Product Line:
ION6200 and ION7300 series meters.

Environment:
ION6200 and ION7300 current inputs.

Cause:
A user require the information on ION6200's and ION7300's nominal current.

Resolution:
The nominal current of both ION6200 and ION73xx are both 5A. The installation guides of these meters only list their rated current at 10A RMS. However, rated current is different from the nominal current which is determined by minimum current that meets the claimed accuracy standard, such as IEC62053-22 and IEC60687.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings