Issue:
In Vista, a background or icon is displayed correctly, however, in webreach/Diagrams only a red X is displayed.
Product:
ION Enterprise 6.0
StruxureWare Power Monitoring 7.0
Power Monitoring Expert 7.2/8
Cause:
The program cannot display a file in Webreach/Diagams if name contains special characters such as "&".
Resolution:
Change the name of the file to alphanumeric charaters only.
Released for: Schneider Electric Nigeria
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.