How can we help you today?

Can ION Setup 3.0 be used to generate a phasor diagram for a ION 7350?

Issue:
User would like to view phasor diagrams for the ION7350 meter using ION Setup 3.0

Product Line:
ION7350 Meters, ION Seutp 3.0

Environment:
Power Metering, Meter Setup Software

Resolution:
ION Setup does not support phasor diagrams on the 7350. As the latest firmware version 7350V285, there is no phasor diagram support for that meter. Use the phasor tool for ION meters found in Meter Wiring Diagnostic Tool (Phasor Diagram, Phasor Tool) to generate a phasor diagram for the ION7350

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: