Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What quantities are logged in the ION_Data database for Alarm Web configuration?

Issue
PME Alarm Web Configuration does not show digital inputs or Alarms created from digital inputs do not populate within Web Applications

Product Line
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0+
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
SQL Server Management Studio

Cause
The digital input needs to map to a measurement that PME can resolve.

Resolution
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*

The following query returns all the quantities being logged, including the ones in VIP.
USE ION_Data

SELECT s.Name SOURCE_NAME, r.Label RECORDER_NAME, c.Label CHANNEL_NAME, q.Name QUANTITY_NAME
FROM Source s INNER JOIN Recorder r
ON s.ID = R.SourceID INNER JOIN Channel c
ON r.ID = c.RecorderID INNER JOIN Quantity q
ON c.QuantityID = q.ID

order by s.Name, r.Label, c.Label

Below is a sample of the result set:
PME8 Alarm

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: