Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How can I view hidden system graphic pages PowerSCADA Expert

Issue
When you attempt to search for a System page in Graphics Builder from File>Open, you can not locate them.

Product
Powerlogic Scada 7.1/7.2
PowerSCADA Expert 7.3/7.4/ 8.x
EcoStruxure™ Power SCADA Operation 8.2

Environment
Graphics Builder pages search function

Cause
System pages are prefixed with an exclamation mark (!) and are not normally visible when searching for Graphics pages.

Resolution
In order to view these pages you need to ensure that you select 'List System Pages'. To set this property, navigate to Tools>Options in Graphics Builder and ensure that 'List System Pages' is checked.

Options

The following video demonstrates this procedure: