How can we help you today?

ENM 7.1 Individual Onboard Alarms Not Showing

Issue

Users would like to see individual onboard alarms from each of the devices in the ENM Filter. The VIP Alarms and the Alarm Sentry Alarms will show up; the default alarm tags from the devices will not show up. Only the group names and the device names show up in the ENM Filter.

Alarm Filter

Product

Event Notification Module 7.1

Power Monitoring Expert 7.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Enviorment

ENM Filter

Resolution

ENM does not talk directly to the meters. ENM receives alarm data from SPM/PME from OPC values or events recorded in the global event log. If a specific alarm is required, the user will need to expose this alarm in OPC via the VIP. If the alarm state can transition quickly, consider setting up a latching alarm.

Note: As of Pme 2021, ENM has been integrated as a function of the Web Application.https://product-help.se.com/docs/EcoStruxure/Power-Monitoring-Expert-2024/content/4_configuring/webapps/event_notification/eventnotification_config.htm?Highlight=ENM

Recommendation:

If you are using an older version of PME, consider upgrading to the latest version for improved protocol support and security. For assistance with integration or upgrades, contact Schneider Electric Technical Support at: pmo.support@se.com

recommendation to upgrade PME

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: