Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I get the time stamp information for the minimum or maximum values which I can see from the front panel of the Circuit Monitor Series 2000 ?

You will need System Manager Software to see the time stamp of minimums and maximums in the circuit monitor min/max log. The time stamps for these minimums and maximum are not stored in registers.

Original article #4044

Legacy KB System (APS) Data: RESL182801 V1.0, Originally authored by KBAdPM on 03/15/2007, Last Edited by KBAdPM on 03/15/2007
Related ranges: CM2000

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings