Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to set the system type of an Enercept Meter

Product Line
Enercept Meter

Environment
Voltage Mode Setup

Resolution
The factory default for the meter is a system type 40, but the following options are valid:

20 = Single Phase, 2 Wire
21 = Single Phase, 3 Wire
30 = Three Phase Delta
40 = Three Phase Wye

Write one of these values to the Single Holding Register 36.

Reference the video in FA180037 for information on how to write to registers.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings