Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Time Sync a 7300 meter using ION Setup

Goals and Symptoms

Summary
7300 meters do not have a clock module.  This article describes how to time synch the meter using ION Setup.

Facts and Changes

Keywords
sync, synch, synchronize

Causes and Fixes

Resolution

  1. Connect to the meter using ION Setup.  In the system logon screen, the "Single ION device configuration mode" must be unchecked
    ion setup login page
  2. Within ION Setup, right-click on the computer name in the left-hand tree and select "Insert Item" to add a new Site.  Use Serial Port or Ethernet Port depending on network configuration.  With Serial Port configuration, set up link type and link speed.
  3. Add the meter by right clicking on the newly created site, and choosing "Insert Item", then select "Meter".  Select appropriate meter type and unit id or IP address.
  4. Verify meter is connected by selecting a module and viewing live data.
  5. To time sync, click the circular clock time sync button "Broadcast present PC time to devices" icon in the menu bar.
  6. Confirm that the time for the meter, displayed in the top left corner of the window, is the same as the time of the computer to which the meter was synched.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings