{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the 6200 be used as an Ammeter, without any Voltage Inputs?

Yes, the 6200 can be used as an ammeter without any voltage inputs, but there may be some accuracy issues depending on the frequency.

For proper accuracy, the sampling rate is set by the frequency read from V1, otherwise, this value defaults to 60 Hz.  If you are operating this in a 50 Hz environment, you may obtain better accuracy by having a 50 Hz input into V1.  If the power supply is the same as the line frequency, the power supply leads can be connected as follows to inject the proper frequency to the meter:
V1 = L+
Vref = N-
G = G

NOTE: this is a workaround, so we cannot guarantee that the meter will be within specification.  Additionally, the meter will not read correct values for anything other than current.  Values that depend on the Voltage Inputs, such as Power and Energy will not be valid.

Original article#10106
Last Revised: October 30, 2007
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189042 V1.0, Originally authored by KBAdPM on 11/09/2007, Last Edited by KBAdPM on 11/09/2007
Related ranges: ION6200

Schneider Electric Nigeria