Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there any surge protection for the Ethernet communications on the ION meters?

ION meters have isolation on the Ethernet ports of the communication cards for any kind of surge. They are transformer isolated with a minimum isolation voltage of 1500VAC/2250VDC.

Last Revised: April 9, 2008
Applies To: ION 7330 / 7350, 7550 / 7650, 8600, 8800
Original Author: KG
Public
All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL191641 V1.0, Originally authored by KBAdPM on 04/10/2008, Last Edited by KBAdPM on 04/10/2008
Related ranges: ION8800, ION8600, ION7550/ION7650, ION7300, ION6200