Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
3720 Snapshot Log Causes Events in ION Enterprise Syslog

Goals and Symptoms

The meter's Snapshot Recorder has been configured into a state that causes many warning events to be recorded in the System Log of ION:Enterprise, as per:

Screenshot reads:

  • System Events Details
    Prioity WARNING
    Source LOGINSERTER.<computer_name>
    Target
    Category Database General
    Computer <computer_name>
    Description 0xa210@<meter_name> - failed to insert records 0 through 0 because 'Index was outside the bounds of the array.'. Will retry in 60s.

This has been traced to the snapshot recorder having source inputs but no depth to record into. We have not determined what allowed this configuration to occur, but we do have a resolution.

Causes and Fixes

Connect to the meter in ION Designer or ION Setup and open the Snapshot Recorders setup parameters

  1. Identify the particular Snapshot Recorder that has source inputs but no depth.
  2. You will need to add depth to the Data Recorder before it will allow you to disable the sources.
  3. Once you have created a depth of at least 1 record, you will be able to delete the sources of the recorder.
  4. Reduce the number of records back to 0. This will disable the snapshot recorder, and prevent the warning from populating the system log.



Last Revised: April 17, 2008
Applies To: ION Enterprise, 3720 ACM
Original Author: LS
Public
All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL191706 V1.0, Originally authored by KBAdPM on 04/18/2008, Last Edited by KBAdPM on 04/18/2008
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, 3720 ACM