Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
The ION 75xx RTU reads -1 for all external numeric registers and will not save any changes after a register write

Issue
User is getting -1 when reading an externa numeric register. The user may notice that any changes to this register will not save

Product Line
ION 7550 and ION7500 RTU

Environment
ION Framework

Cause
The ION 75xx RTU units do not come with predefined framework on the meters. If a module does not exist on the framework, modbus requests will return -1.

Resolution
Use ION Setup or ION Designer to create external numeric modules and unlock the registers. Once the module has been created the register will read 0 instead of -1.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings