No, certain energy levels meet the 0.2 accuracy standards (kVAh, kWh), but others fall short (kVARh). Since all parameters do not meet the standard it is not possible to classify the meter with the C12.20 class 0.2 accuracy standard.
Released for: Schneider Electric Nigeria