Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a global library of Genies be created that is accessible from all projects within Powerlogic SCADA?

No, a global library of Genies cannot be created such that it is accessible to more than one project. However, a project can be created that serves as a host of standard and common Genies that a user may want to incorporate into multiple projects. This project (e.g. ES_Common or ES_Oneline) can then be added into any other project as an Included Project (Citect Project Editor > System > Included Projects). Once the project is included, it's library of Genies are now accessible by the project to which it is included.


Legacy KB System (APS) Data: RESL199126 V2.0, Originally authored by KBAdPM on 06/10/2009, Last Edited by MaTh on 12/02/2010
Related ranges: PowerLogic SCADA 7.1