Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Uses of the PT/CT ratio on E5600

Goals and Symptoms

This article explains the importance of PT/CT ratio on E5600 meter.

Causes and Fixes

On the E5600 the PT/CT ratios do not have any effect on the rate of pulses. The PT/CT ratios only affect values shown on the meter display and through MODBUS. By default the PT/CT ratios are set to 1, use this ratio to see what the meter is measuring on its blades or secondary side.
When the voltage and current that the meter is monitoring at the secondary side of the PT/CTs is low it will take time before the KWh, kVARh, kVAh etc., in the real time screen, will show some values. In the example in Figure 1 and 2 there are no values for KWh, KVARh and kVAh even after five minutes. Same is true for the values displayed on the screen. Only integer values are displayed in the real time module and the meter display. In order to see the values that are less than 1 KWh/KVARh/ kVAh increases the PT/CT ratios and keep in mind that the new energy values have scaling.

Figure 1
Figure 1


Figure 2
Figure 2

Figures 3&4 below show the voltage and current applied to the 16S E5600 meter in the above example.

Figure 3

Figure 3

Figure 4

Figure 4

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: