Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
“Use GPS Quality Flag,” has been introduced in the Setup Register for ION8600 version 332 ( v332).

Issue

For some reason, unexpectedly the meter (ION8600) stops communicating.

Product Line

ION8600

ION Setup

Environment

Configuration

Cause

The clock source couldn’t sync.

Resolution

A new setup register has been added to the clock module on the ION8600 v332. This register is called Use GPS Quality Flag and provides two configuration options: Use Flag and Ignore Flag.

In previous firmware versions, meters configured to synchronize with a GPS time source would only accept time synchronization when the GPS was locked to a satellite. If the GPS source became unlocked, the meter would stop accepting time sync signals until the lock was restored.

Go to ION Setup Advanced configuration > Clock Modules  > Setup register. See highlighted on figure 1 below.

Fig. 1

Figure 1

To select one of the behaviors: Highlight CL1 Use GPS Quality Flag  > Edit   > Then select either one. See figure 2 below:

This new feature allows users to choose between two behaviors:

Use Flag: The meter will only accept time synchronization if the GPS source quality flag indicates a locked state.

Ignore Flag: The meter will accept time synchronization regardless of the GPS source quality flag state.

Fig. 2

Figure 2