Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the definition of 'Error State' in Project Color Change Tool

Issue
Project Color Change tool will give you information on the busbar/circuit breaker through different color coordinations

Product Line
PowerLogic SCADA 7.1

Environment
Ecostruxture Power Operations

Resolution
It means communication error only for circuit breakers. It doesn't mean any H/W error or logic error on your devices / ED networks.

project color change tool