Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION8300 Meter Template Files

Product Line
ION8300

Environment
Templates

Resolution
You can install meter templates using ION Setup. See the "Upgrading ION Device Firmware" technical note for complete details.

Install Templates with ION Setup

  1. Download the device template and save it to your ION Setup TEMPLATE folder (select the file below that matches your meter's feature set).

Use these .DCF files with ION Setup to perform firmware upgrades. These are default meter templates only. If you have custom programming in your meter, create your own template file before performing the firmware upgrade.

  1. Follow the upgrade procedures outlined in the Upgrading ION Device Firmware technical note.

See the .zip below for the following templates:

VersionClass 2 (1 Amp)Class 20 (5 Amp)
V264-2658300_FAC-9S-36S_V2.6.0.0.9
8300_FAC-35S_V2.6.0.0.9

V2628300_FAC-9S-36S_V2.6.0.0.2
8300_FAC-35S_V2.6.0.0.2
V2448300_v240_FAC-C2A-9S_V1.4.0.0.1
8300_v240_FAC-C2A-35S_V1.4.0.0.1
8300_v240_FAC-C2A-36S_V1.4.0.0.1
8300_v240_FAC-9S_V1.4.0.0.1
8300_v240_FAC-35S_V1.4.0.0.1
8300_v240_FAC-36S_V1.4.0.0.1

Schneider Electric Nigeria

Attachment(s)
8300_Templates.zip [600.16 KB]