{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
StruxureWare Power Monitoring 7.0.1: SQL Server 2005 Standard Edition Upgrade Guide

Goals and Symptoms

StruxureWare Power Monitoring requires a compatible version of SQL Server. It is possible to do an in-place upgrade of SQL Server 2005 to a supported SQL Server version. This is a prerequisite for an upgrade from ION Enterprise to StruxureWare Power Monitoring 7.0.1.

Causes and Fixes

The attached document describes how to perform an in-place upgrade of SQL Server 2005 Standard Edition for both Stand Alone and Distributed ION Enterprise system in preparation for an upgrade to StruxureWare Power Monitoring 7.0.1. This document does not address the case where an existing ION Enterprise system is using SQL Server 2005 Express Edition. For this case, see RESL207643.

Attachments

(Removed File URL: 207632_2ABA/SPM701-SqlStandard2005UpgradeGuide.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/645e981c4463073ec1257a620010c2eb/fl_block_5/0.200?OpenElement&FieldElemFormat=gif)
(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/645e981c4463073ec1257a620010c2eb/fl_block_5/0.3DEC?OpenElement&FieldElemFormat=gif)
Last Revised: August 21, 2012

Internal

All content © 1992-2012 Schneider Electric


Legacy KB System (APS) Data: RESL207632 V8.0, Originally authored by MaLi on 03/13/2012, Last Edited by JaMc on 08/22/2012
Related ranges: Power Monitoring 7.0

Schneider Electric Nigeria

Attachment(s)
SPM701-SqlStandard2005UpgradeGuide.pdf [617.67 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.