Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Configuring Waveform recordings on the PM800 series meter with ION Setup software
Issue
Need to configure the waveform capture on a PM800 series meter.

Product Line
PM850, PM870, ION Setup

Environment
Application using a PM800 series meter to capture waveforms

Cause
Need configure waveform capture on a existing PM850 or PM870

Resolution
Both the PM850 and PM870 can capture waveform data. Capture can be enabled in the Onboard Alarms/Event setup, see figures below.

ION Setup

ION Setup display of Alarm setup

The PM870 can configure aspects of the waveform like the channels selected, samples per cycle, duration, and pre-event cycles. These values are fixed in the PM850.  The waveform capture configuration is accessed through the Power Quality folder.

PM850 and PM870 waveform capture options
ION Setup Waveform capture options

ION Setup Waveform capture settings

Note

  • ION Setup cannot view waveforms from this device.