Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Launching PowerLogic SCADA 7.10 and 7.20 Web Clients from the Same Workstation or Laptop; Red X or "Can not load citectweb.dll" Error

Goals and Symptoms

In some cases, a user will need to monitor multiple PowerLogic SCADA (PLS) systems from a single workstation or laptop. If one of these systems is version 7.10 and another is version 7.20, some complications may occur when launching one after the other. This article describes each issue and provides a work around process that must be followed each time the user switches between web deployments of the different versions.
Symptoms of running a 7.10 web deployment after running the 7.20 web client:
When the user attempts to run the web client for a 7.10 project after running the web client for a 7.20 project, the following behavior is encountered:
A red X will be displayed in the top left corner of the page and the web client does not appear to attempt to load.


Symptoms of running a 7.20 web deployment after running the 7.10 web client:
The user will receive the following error: "Starting Citect Web Client Failed: Can not load citectweb.dll."

Causes and Fixes

Solution for running a 7.10 web deployment after running the 7.20 web client:

1) Close all instances of Internet Explorer (IE).
2) Delete the Citect folder from C:\WINDOWS\system32. The attached batch file will accomplish this for a Windows XP operating system.
Delete_Citect_folder_from_System32.batDelete_Citect_folder_from_System32.bat

For clients that have windows 7 or 2008 operating system use the following batch file to delete the Citect folder folder from C:\Windows\SysWOW64

Delete_Citect_folder_from_System64.bat

3) Reopen IE and launch the webclient for the 7.10 project. The proper cab file for the web client will be installed and the web client should successfully launch.

Solution for running a 7.20 web deployment after running the 7.10 web client:

1) Close all instances of IE.
2) Delete the Citect folder in the temp folder (Go to run, type %tmp% and click OK, then delete the Citect folder).
3) Run the web client for the 7.20 project. The cab file will be installed the first time and the web client should successfully launch.

Keywords: PLS, PLSCADA, PL SCADA, PowerSCADA, Power SCADA, StruxureWare PowerSCADA Expert, PSE, SPE 7.2, 7.20, 7.1, 7.10


Legacy KB System (APS) Data: RESL209571 V3.0, Originally authored by AnVa on 11/05/2012, Last Edited by RaDe on 07/29/2013
Related ranges: PowerLogic SCADA 7.1, PowerSCADA Expert 7.2