{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the Auto-tuning requirements for a Twido PID function?

Issue:
Auto-tuning requirements for a Twido PID function


Product Line:
TwidoSuite


Resolution:
The Auto-tune requirements for a Twido PID function are listed below:
1. The control process must be an open-loop, stable system.

2. At the start of the auto-tuning run, the control process must be in steady state with a null process input (e.g.: an oven or a furnace shall be at ambient temperature.)

3.During operation of the auto-tuning, make sure that no disturbances enter through the process for either computed parameters will be erroneous or the auto-tuning process will simply fail (e.g.: the door of the oven shall not be opened, not even momentarily.)

4. Configure the Twido PLC to scan in Periodic mode. Once you have determined the correct sampling period (Ts) for the auto-tuning, the scan period must be configured so that the sampling period (Ts) is an exact multiple of the Twido PLC scan period.

Schneider Electric Nigeria

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.